Browse FAQs

What is the part number for the Advantys STB screwdriver?

Published date: 28 January 2019

The part number for the Advantys STB screwdriver is STBXTT0220. This screwdriver is slotted with fully insulated chrome vanadium steel shaft, .4mm x 2.5mm tip, 75mm blade length, overall length 179mm, 1,000v protection certified.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.