Browse FAQs

Does the RJ45 protector plug need to be installed on the ruggedized Modbus plus tap 990NAD23010 in order for it to work?

Published date: 25 September 2018

YES. The RJ45 protector plug should be in place to protect the programming port from harmful elements and to establish a positive connection to the RJ45 port pins. When the programming cable is removed, and the RJ45 protector plug is install, it establishes a positive connection to the movable pins inside the RJ45 connector to complete the circuit.



Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.