Browse FAQs

What are the Front Cover part numbers for the Compact A120 Series rack and I/O assemblies?

Published date: 28 January 2019

There are two different Front Covers. The five slot backplane cover is 043507935. The two slot backplane cover is 043507936.
These parts are only available through our service sales department. They can be contacted either via email at service.sales@us.schneider-electric.com or 1-888-266-8705 option 2.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.