Browse FAQs

What Remote I/O adapters require an external in-line terminator?

Published date: 13 June 2019

Issue:
Determining what RIO modules require an external in-line terminator.

Product line:
984 800 series and Motion controllers

Cause:
There are RIO heads that do not require the external RIO terminator and list provides thee ones that do require it. 
Resolution:
The devices listed below have no built in terminator and require an in-line terminator, PN 60-0513-000 installed in the drop cable.

RIO Drop adapters
text
AS-J890-001
AS-J890-002
AS-J892-001
AS-J892-002
410 Motion Controllers
110-230
110-232
110-231
110-233
3240 Motion Controllers
100-265-815
100-265-816
100-265-825

Note: The above products are all obsolete and an upgrade would be recommended. Also to switch from RIO to Ethernet.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.