Technical FAQs

Ask a Question

Can I convert several consecutive words to a bit level using a single Concept function block?

Yes. The IEC_BMDI in the LIB984 allows the programmer to convert up to 100 consecutive words to a bit level or up to a 1000 bits to a word level by simply using a single function block. This block is available in Concept Version 2.2 and above using IEC.

Here is an example to program the IEC_BMDI block


Legacy KB System (APS) Data: RESL121918 V2.0, Originally authored by RiTa on 06/29/2012, Last Edited by GeMc on 06/29/2012
Related ranges: Concept
Was this helpful?
What can we do to improve the information ?