Browse FAQs

Why does the wiring diagram of my Momentum I/O base show more rows of terminals than are actually on the base?

Published date: 31 October 2018

The diagram is showing the use of bus bars, which are optional and mount directly to the IO base. These bus bars may be used to assist with the wiring of 3 and 4-wire field devices. Each row of terminals are connected or bussed internally.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.