Technical FAQs

Ask a Question

Is there a Modbus Tap that provides Isolation and Pre-polarization?

Yes, the TWDXCAISO Modbus tap provides RS485 line isolation, Line end termination, and RS485 Line pre-polarisation.
Below is attached the installation manual for the TWDXCAISO Modbus tap.

 

Was this helpful?
What can we do to improve the information ?