Technical FAQs

Ask a Question

When can the IP address be assigned to a High End Quantum CPU Ethernet port through the LCD pad?

The IP address can be assigned to the CPU Ethernet Port through the LCD pad, only when the CPU is in a No Configuration condition.
The LCD screen will display the term "NO CONF" when there is no configuration on the CPU.


Note: The Unity Quantum processors will be obsoleted 12/31/2018 and the recommended replacement is the M580, for more information on this contact your local distributor or Schneider offic. 
Was this helpful?
What can we do to improve the information ?