Browse FAQs

Does the Momentum PLC support the ODVA Ethernet/IP protocol?

Published date: 23 August 2019

Issue:
Does the Momentum Processors support the ODVA Ethernet/IP protocol?

Product line:
Momentum, Unity Momentum

Cause:
Questions on weather or not the Momentum will support the OVDA Ethernet IP protocol.

Resolution:
No, the Momentum PLC does not support the ODVA Ethernet/IP protocol. The Momentum only supports the ModbusTCP protocol via a Ethernet connection.


Note: The Momentum line is now only the Unity Momentum processors, all other processors are obsolete.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.