Technical FAQs

Ask a Question

Where can I download the A120 hardware reference manuals?

 

 
Here is the userguide to the A120 line.  The PLC hardware guide will be included in the first link, and the A120 I/O hardware manuals are in the second link.
 
 
http://eclipse.modicon.com/85256CBB0074C0EF/C7720116867B3CFD85256CBC0068AD59/649FF55CF897937F85257B3B006FA8ED
 
http://eclipse.modicon.com/85256CBB0074C0EF/C7720116867B3CFD85256CBC0068AD59/8A34E9F3C9D10D5A852578D200627617
Was this helpful?
What can we do to improve the information ?