Browse FAQs

Why do many of the internal elements of the Control Expert 14 (formerly named Unity Pro) T_ANA_IN_BMX IODDT appear to be unresponsive when viewed in logic?.

Published date: 30 September 2019

The T_ANA_IN_BMX IODDT works in conjunction with the READ_STS block. Configure a READ_STS block for the appropriate IODDT and it will then update all elements.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.