Technical FAQs

Ask a Question

When using ProWORX 32 what is the maximum number of configurable words in the local Quantum drop?

In applications configured with PW32 (also ProWORX NxT) the maximum number is 64 input & 64 output words.
Thiese values are specific to the Quantum RIO drop. 


Legacy KB System (APS) Data: RESL212333 V1.0, Originally authored by RoAl on 08/20/2013, Last Edited by RoAl on 08/20/2013
Related ranges: Unity Pro - SoCollaborative software
Was this helpful?
What can we do to improve the information ?