Technical FAQs

Ask a Question

How can the error message "Unable to open bin file." when flashing Unity Quantum firmware be corrected?

This is usually caused when using the incorrect communication protocol. For example, when flashing the executive firmware on a Unity Quantum PLC, you must use Modbus or Modbus Plus communications.


Legacy KB System (APS) Data: RESL212302 V1.0, Originally authored by DaSo on 08/14/2013, Last Edited by DaSo on 08/14/2013
Related ranges: Unity Pro - SoCollaborative software
Was this helpful?
What can we do to improve the information ?