Technical FAQs

Ask a Question

In Vijeo Designer, is there a way to cross reference all variables and where it is being used?

Yes, you can cross reference all variables used in Vijeo Designer. Below is the instructions on how to get the report:
1 - Select (highlight) the variable node

2 - Goto the Report Menu and select Variables..

3 - Select Yes

4 - Change the Variable Report to "cross reference all variables by name" and select OK

5 - Then the list will be generated.


Was this helpful?
What can we do to improve the information ?