Browse FAQs

Can I flash the executive firmware to a 984LL Quantum controller over the backplane through a Quantum NOE?

Published date: 11 June 2019

No, you can not flash the firmware exec to the 984LL Quantum controller through the backplane from the Quantum NOE.
You have to connect directly to the controller using either the Modbus or Modbus Plus communication protocol.



Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.