Browse FAQs

Why do I get an error: "specified address invalid" when trying to communicate to a Rockwell PLC from a Magelis via Ethernet/IP?

Published date: 28 December 2018

The problem was in Rockwell's RSLogix 5000 software. In RSLogix 5000, tags (variables) can be setup to have "External Access". There are three options for "External Access" to either None, Read Only, or Read/Write. If the tags are setup as "None", the HMI will not be able to communicate with the PLC. You need to set the tags up for "Read/Write" in order to get communications between the Magelis and Rockwell PLC.



Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.