Browse FAQs

Does the HMISTU655/855 supports the GE protocol?

Published date: 30 May 2019

Issue: 
Does the HMISTU655/855 supports the GE protocol?


Product Line:
Vijeo Designer, HMISTU


Resolution:
The HMISTU655/855 does not support the GE protocol. The reason for this is because the GE PLC requires all the
flow control pins. As the RJ45 connection doesn't allow for this, the HMISTU cannot communicate to the PLC.

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.