Browse FAQs

172JNN21032 MB option adapter used with Momentum CCC980 30 PLC. Cannot configure the MB port on the adapter.

Published date: 29 March 2019

When this option adapter is assembled with a CCS78000, CCC78010 or CCC98020/30 PLC, its Modbus port (port 2) is electronically disabled. The TOD clock and the battery backup on the option adapter remain functional.



Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.