Technical FAQs

Ask a Question

Unity Pro: Launching app. causes error: "Impossible to find the Unity Pro common application path."

Open the Registry Editor (regedit) and check the for the following key.
HKEY_LOCAL_MACHINE\SOFTWARE\Microsoft\Windows\CurrentVersion\Explorer\Shell Folders\Common AppData

Add this key if it does not exist. To add the key, do the following:
Right click on ShellFolders and choose New - Key. Type Common AppData. Double click on this and add the 'Value Data'. Set this value to C:\Documents and Settings\All Users\Application Data.

Was this helpful?
What can we do to improve the information ?