Technical FAQs

Ask a Question

Unity Pro update, incidence on SFC in multi-token application: Maximum number of active steps/section and actions/section calculation

Goals and Symptoms

On updating Unity Pro V5.x (or lower) to V6.0 (or upper), for SFC application using multi-token mode, it can be needed in some situation to re-adjust the Maximum number of active steps/section and actions/section setting, rebuild and redownload the application.

Example of message which can occur after openning a STA or rebuilding the application.
{Chart : [MAST - Sfc secrion name]} : E2554 maximum number of active steps is set to '40', but must be at least '47'

Facts and Changes

Maximum number of active steps/section and actions/section setting have to be adjusted in the menu Tools->Project Settings

Causes and Fixes

The calculation of the maximum number of active steps/section and actions/section has been corrected since Unity Pro V6.0, it was previously uncorrect and could lead to application execution issue.
As consequence, on an Unity Pro update from Unity Pro V5.x (or lower) to V6.0 (or upper) :
The project setting : maximum number of active steps/section and actions/section can be needed to be re-adjusted and in some case if the limits of 100 are reached, the SFC section which have reached the limits have to be splitted 2 or several sections.


Legacy KB System (APS) Data: RESL210571 V1.0, Originally authored by ChAn on 02/07/2013, Last Edited by ChAn on 02/07/2013
Related ranges: Unity Pro - SoCollaborative software
Was this helpful?
What can we do to improve the information ?