Browse FAQs

HMISTU655 is missing the power connector. Is there a part number for the power connector?

Published date: 30 May 2019

Issue: 
Is there a part number for the missing power connector for the HMISTU655

Product Line:
HMISTU


Resolution:
Yes, the part number for the HMISTU655 power connector is XBTZGPWS1. This part comes in a set of 5 connectors.

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.