Browse FAQs

Is there a maximum limitation on the XBTGT series for Compact Flash card size?

Published date: 10 May 2019

Issue: 
maximum limitation on the XBTGT series for Compact Flash card size

Product Line:
XBTGT

Environment:
N/A


Resolution:
The maximum size of CF card that the XBTGT series can handle is 2GB. This is due to the limitation of the hardware.
FYI: The HMIGTO series can handle larger capacity SD cards .


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.