Browse FAQs

Can a BMXNOM0200 module work with a BMXPRA0100 ?

Published date: 30 September 2019

Title
Installing a BMXNOM0200 in a  BMXPRA0100 
 
Issue
BMXNOM0200 compatibility

Product Line
M340
 
Environment
Unity Pro
 
Resolution
Yes, however the BMXPRA0100 needs to be using firmware version 2.3 or greater and the BMXNOM0200 needs to be using firmware version 1.2 or greater


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.