Technical FAQs

Ask a Question

What are the differences with the M340 BMXCRA312x0 adapters ?

Release Notice

These modules require the use of Unity 7.0 or higher.

Goals and Symptoms

Explain the difference between the two M340 QEIO Remote Drop adapters that can be used in a Quantum Ethernet IO system.

Facts and Changes

Requires the use of Unity 7.0 or higher and the use of a version 1.5 QEIO 140CRP31200 module.

Causes and Fixes

Listed below are the differences between the BMXCRA31200 and the BMXCRA31210 Adapters.
Only the BMXCRA31210 has the addition of a Service port. See below.




Listed below are the different type/number of I/O supported by the BMXCRA31200 and the BMXCRA31210 Adapters.



 


Legacy KB System (APS) Data: RESL209823 V1.0, Originally authored by BrWa on 11/30/2012, Last Edited by BrWa on 11/30/2012
Related ranges: Modicon M340
Was this helpful?
What can we do to improve the information ?