Browse FAQs

What are the Minimum System requirements for installation of Concept 2.6?

Published date: 01 April 2019

- PC with Intel Pentium CPU or better
- Minimum of 24 MB Ram or more
- Minimum 150 MB free hard disk space
- CD ROM drive
- SA85/PCI85 module if Modbus Plus is being used
- TCP/IP Network card if Ethernet is being used
- VGA graphic card, and monitor (at least 800x600)
- Microsoft compatible mouse
*Concept 2.6 SR7 will run on Windows 7 32 bit. No plans for 64 bit support.


Legacy KB System (APS) Data: RESL209329 V1.0, Originally authored by GeMc on 10/08/2012, Last Edited by GeMc on 10/08/2012
Related ranges: Concept

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.