Technical FAQs

Ask a Question

Can the Magelis XBTGT communicate with the AB MicroLogix 1100 controller over ethernet?

The AB MicroLogix 1100 uses a variation of the supported MicroLogix Ethernet protocol. Engineering reports the AB MicroLogix 1100 was tested and is supported.

Was this helpful?
What can we do to improve the information ?