Browse FAQs

Unable to connect to Unity simulator Windows 7 64 bit. "This isn't a valid PLC Address, or PLC is busy, or media is off."

Published date: 11 December 2018

When using Win7 OS, the desktop theme can affect the simulator.
Right click on the desktop and go to <Personalize>.
Make sure that you are choosing a Windows 7 Basic theme. Aero or high contrast themes can cause a problem.



Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.