Technical FAQs

Ask a Question

How do I convert a Modsoft database to ProWORX NxT?

Goals and Symptoms

The following procedure will show you how to convert the Modsoft Database called "Example" to a ProWORX NxT database named "Example".

Causes and Fixes

Run the NxT Convert Utility. From the START menu select "Programs" - "ProWORX" - "NxTConv".
Choose the option for "Convert Modsoft database to NxT"


Select a database for the source - this will be your Modsoft database to be converted.



Enter a new database name for the destination - this will be your NxT database.


You will get a message window asking you to create a new NxT file, select the YES button.


Click the Start button to begin the conversion.

Was this helpful?
What can we do to improve the information ?