Browse FAQs

How come the blink color animation of a rectangle is grayed out in Vijeo Designer for Magelis XBTGT screens?

Published date: 05 July 2019

Issue: 
The blink color animation of a rectangle is grayed out in Vijeo Designer for Magelis XBTGT screens


Product Line:
Vijeo Designer, Magelis XBTGT


Resolution:
In order to get the blink color animation to be active, you need to change the TargetColor type from "64K color" to "16K with blinking". TargetColor
is located in the Property Inspector window of the Target1.



Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.