Browse FAQs

How many Modbus TCP/IP connections can the Advantys STBNIP2311 manage?

Published date: 16 August 2019

Issue: 
Modbus TCP/IP connections supported by the Advantys STBNIP2311 NIM


Product Line:
Advantys, STBNIP2311


Resolution:
The STBNIP2311 can manage a maximum of 16 Modbus TCP/IP connections.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.