Browse FAQs

Can the BMXNOE0100 I/O scan the BMXPRA0100(Peripheral Remote IO Adaptor)?

Published date: 27 September 2018

Yes, the BMXPRA0100 can be IO scanned by a BMXNOE0100. When setting up the NOE IO Scanning in the M340 project, you can launch a new instance of Unity Pro from within the IO scanner configuration by selecting the ellipsis in the Device Name field. Whatever name you enter for the Device Name will be the Unity Pro project name for the BMXPRA0100. This is the only thing that this Device Name will be used for is the Unity Project name, unlike linking a DTM which can use it as a Role Name.

It is not necessary to link the Unity Project to the Device Name column, but the value add is being able to launch the PRA configuration right from the IO scanner line rather than manually searching for the correct PRA project in the future.

 

 


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.