Browse FAQs

What is the communications cable between Magelis XBTN401/N410/NU400/R410/R411 and the Unity Quantum 140CPU65150/65160/67160 controllers?

Published date: 05 July 2019

Issue: 
communications cable between Magelis XBTN401/N410/NU400/R410/R411 and the Unity Quantum 140CPU65150/65160/67160 controllers


Product Line:
Magelis XBTN/R, Quantum 140CPU65150/65160/67160


Resolution:
XBTZ9711 is the communications cable between the XBTN/R and a Unity Quantum controller. This is a RS232 communication.



Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.