Technical FAQs

Ask a Question

Why do I get ProWORX NxT error "database is being used by another user"?

Check to see if you have a ProWORX NxT database file with a *.$$$ extension. *.$$$ are temporary files that are created when the ProWORX NxT database is in use. If the database is not in use, you should not see these files. If your PC crashes while NxT is in use, the *.$$$ files will remain with the project files. Delete the *.$$$ file and this will get rid of the ProWORX NxT "database is being used by another user" error.

Was this helpful?
What can we do to improve the information ?