Browse FAQs

Why do I get an "EZPDLL caused a general protection fault" error when trying to install service releases to ProWORX NxT v2.20?

Published date: 29 November 2018

Issue
"EZPDLL caused a general protection fault" error

Product Line
ProWORX NxT

Cause
Installing a service release to ProWORX NxT v2.20

Resolution
Place the service release file in the C:Proworx\Nxt folder and run it from there. The service release will install successfully without giving you the "EZPDLL caused a general protection fault" error.

 

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.