Technical FAQs

Ask a Question

Can you down-load a Vijeo Designer application to a XBTGT over the internet?

If the target has its own external IP address, then it is possible to down-load an application via the Internet. (But you should probably enable down-load security in that case.)
If you need to connect to the target indirectly through a router with port forwarding, down-loading an application to the target is not possible.

Was this helpful?
What can we do to improve the information ?