Browse FAQs

Why does Vijeo Designer version 4.6.0 show Function Keys for a target that does not have them?

Published date: 23 August 2019

Starting with Vijeo-Designer 4.6.0, any target with a USB port, supports USB input devices (keyboard and mouse).
These targets can use the "Function Keys" feature as it is related to the function keys on the USB keyboard.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.