Browse FAQs

What devices (computers, Fieldbus, software) are compatible with the TSXCUSBFIP adapter?

Published date: 04 June 2019

Issue
Device and software compatibility with the TSXCUSBFIP

Product Line:
Fipway,TSXCUSBFIP, Vijeo Designer, OPC Factory Server, PL7 pro, Unity Pro


Resolution:
The following tools (hosts) are compatible with the TSXCUSBFIP:
Personal Computer
industrial Personal Computer (Magelis iPC and other iPC)
dialog operators (All Magelis XBTGT/GK except XBTGT1100 and XBTGT1130)


The TSXCUSBFIP communication adapter is compatible with the following:
Networks or field buses:
-FIPWAY
-FIPIO
-WorldFIP

Software:
-Unity Pro V3.0 or higher
-PL7 V4.5 or higher
-OPC Factory Server (OFS) V2.32 or higher
-Vijeo Designer V4.6 or higher


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.