Technical FAQs

Ask a Question

How do I determine the Concept IEC project scan time using a PLC?

Goals and Symptoms
The goal of this resolution is to show the customer how to determine their IEC Concept project scan time.
Causes and Fixes
Once you open the Concept project and connect ONLINE/EQUAL to the controller, make sure that the controller
is running. To view the scan time, you will need to go to the <Online> Menu and open <Memory Statistics> as
shown in illustration below.

Once the <Memory Statistics> window is open, you will see the scan time at the bottom of the pop up window as
shown in the illustration below. Hitting the refresh key and logging the scan time will give you an idea of the scan range.


Was this helpful?
What can we do to improve the information ?