Technical FAQs

Ask a Question

Does the M340 Counter (BMXEHC0200) come with connectors?


No. The M340 High Speed Counter (BMXEHC0200) does not come with connectors.

One BMXXTSHSC20 kit must be ordered with each module..

Note:
The BMXXTSHSC20 kit contains:
2 - 16 terminal Spring clamp connectors
1 - 10 terminal Spring clamp connector

Was this helpful?
What can we do to improve the information ?