Technical FAQs

Ask a Question

What is the cable needed to connect a M340 PLC to the XBTGT11xx?

The following cables will connect a M340 PLC to a XBTGT1100 or a XBTGT1130 HMI.
VW3A8306R03 0.3 m
VW3A8306R10 1.0 m
VW3A8306R03 3.0 m


Was this helpful?
What can we do to improve the information ?