Technical FAQs

Ask a Question

Why is Ethernet not an option in the network list when using Unity Software?

If the NOE is not in the configuration or the chosen PLC does not have an Ethernet
port then Ethernet will not be an available network in the list.

Was this helpful?
What can we do to improve the information ?