Technical FAQs

Ask a Question

Is the TSXCUSBMBP Communication Adapter compatible with Modsoft?

Yes, the TSXCUSBMBP Communication Adapter is compatible with Modsoft if bought after October 1, 2007 or the Virtual Serial Port (VSP) Driver is uninstalled and the MBX Driver version 6.00 Update 20070615 in installed.

Note: Hardware is the same.

 
Was this helpful?
What can we do to improve the information ?