Technical FAQs

Ask a Question

Why won't the Smart iPC save configuration and IP Address changes when it restarts?

This is because the EWF manager is enabled. To save the configurations settings, you need to disable the EWF manager
and reboot the Smart iPC. Make the necessary changes. Reboot the Smart iPC and re-enable the EWF manager.

The EWF Manager tool is located in the following directory : C:\Program files\Change EWF State\ChangeEWFstate.exe

Below are a list of configurations that requires EWF manager disabled in order to save changes:

- New applications installation
- New peripheral installation
- New users creation
- Network configuration : IP address, operating mode...
- OS custom : background picture, screen saver...


Legacy KB System (APS) Data: RESL188196 V1.0, Originally authored by RoAl on 09/24/2007, Last Edited by RoAl on 09/24/2007
Related ranges: Magelis Smart
Was this helpful?
What can we do to improve the information ?