Technical FAQs

Ask a Question

How to reset the security password for ProWORX NxT

Goals and Symptoms

How to reset the security password for ProWORX NxT

Facts and Changes

ProWORX NxT

Causes and Fixes


If the security password to ProWORX NxT is lost, the default password can be restored by:

  • Open the ProWORX\NxT folder.
  • Delete the file named 'NxT.dat'

Use the default security password which is no password when start the security editor by
clicking on File\Security.
 
Was this helpful?
What can we do to improve the information ?