Technical FAQs

Ask a Question

What are the current RG-6 RIO component part numbers?

Here is the current available RG-6 media:

Cable 97-5750-000 (Belden 3092A, RG-6 Quad Shield, 1000 ft.)
Connector MA-0329-001
Stripper Tool 490RIO00400
Crimp Tool 60-0544-000 (Use 0.360 crimp).

Was this helpful?
What can we do to improve the information ?