Browse FAQs

How do I apply the Concept IEC O_SCALE function block?

Published date: 09 October 2018


The Concept O_SCALE block can only be used with a corresponding system block and a module block.
It is only available for use with the Quantum and Compact platforms. It cannot be used with Momentum.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.