Browse FAQs

Is there a limit to the number of pages that Web Gate will support in Vijeo Designer?

Published date: 28 September 2018

No, there is no specific amount of pages supported by the Web Gate. If the number of panels in the application allow the application to run properly on the target, it will run properly in Web Gate as well.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.