Technical FAQs

Ask a Question

What are the processor and clock speeds of the current Quantum CPUs?

The following chart lists all current Quantum CPUs and their processor clock speeds:

CPU Model
Processor / clock speed
140CPU11302
186 / 20 MHz
140CPU11303
186 / 20 MHz
140CPU43412A
486 / 66 MHz
140CPU53414B
586 / 133 MHz
140CPU31110
486 / 66 MHz
140CPU65150
586 / 166 MHz
140CPU65160
586 / 266 MHz
140CPU67160
586 / 266 MHz

Legacy KB System (APS) Data: RESL179129 V2.0, Originally authored by RoAl on 06/23/2008, Last Edited by ThVe on 06/23/2008
Related ranges: Modicon Quantum
Was this helpful?
What can we do to improve the information ?