Technical FAQs

Ask a Question

What is the communication cable pinout to connect an HMIGTO to a Rockwell SLC504 PLC using DF1 protocol?

This is the communication cable betweern a Magelis HMIGTO (2000 to 5000 series) to Rockwell SLC505 using DF1 protocol
(DB9 to DB9 connector)

 

Was this helpful?
What can we do to improve the information ?