Technical FAQs

Ask a Question

Can I export a project out of Concept and import the .ASC file into an earlier version of Concept?

Concept 2.5 and Concept 2.6 use the same EFB data interface.  Concept 2.6 .ASC files can be imported into Concept 2.5.
However, there may be features, (e.g. Defragmentation, FDA security, etc.), used in the later version that are not available in the earlier version.

Concept 2.2 uses a different EFB data interface. You cannot import a Concept 2.5/ 2.6 .ASC file into Concept 2.2.

Versions of Concept earlier than 2.2 use another EFB data interface and Concept 2.2 .ASC files may not import properly into these versions.


 

Was this helpful?
What can we do to improve the information ?